:MEASure:LLINe:LINE:MARGin:STATus?

Query Syntax

:MEASure:LLINeN:LINEM:MARGin:STATus?

Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.

Where M identifies one of 16 {1:16} possible limit lines.

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

Queries the status of the :MEASure:LLINe:LINE:MARGin? measurement for an specific limit line. Use the :MEASure:LLINe:MARGin:STATus:REASon? child query to determine the reason for an invalid or questionable measurement.

See Also