:MEASure:LLINe:LINE:MARGin:STATus:REASon?
Query Syntax
:MEASure:LLINeN:LINEM:MARGin:STATus:REASon?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Where M identifies one of 16 {1:16} possible limit lines.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for a failed :MEASure:LLINe:MARGin? measurement. If the measurement was successful, a null string is returned. Use the :MEASure:LLINe:MARGin:STATus? parent query to determine if the measurement has failed.