:MEASure:LTESt:ACQuire:COUNt?

Query Syntax

:MEASure:LTESt:ACQuire:COUNt?

Description

Use this query to return the current waveforms, patterns, or samples counted when a waveform, pattern, or samples acquisition limit test is enabled (:LTESt:ACQuire:STATe command). This is the count that is shown in Infiniium's upper-right corner. The following commands are used to specify the count number:

The current count can be helpful in instances where acquiring the specified number of waveforms, patterns, or samples takes some time and you need to estimate the completion time.