:MEASure:MTESt:HRATio:STATus?
Query Syntax
:MEASure:MTESt{N}:HRATio:STATus?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of the HRatio measurement. Use the :MEASure:MTESt:HRATio:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:MTESt:HRATio:STATus:DETails? child query.