:MEASure:PJITter:TABLe:DMAXimized

Command Syntax

:MEASure:PJITterN:TABLe:DMAXimized {ON | OFF | 1 | 0}

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Query Syntax

:MEASure:PJITterN:TABLe:DMAXimized?

Query Response

{1 | 0}

Description

When PAM Jitter tables are displayed in a grid (see :MEASure:PJITter:TABLe:GSIZe), this command lets you maximize the most recently selected table (see :MEASure:PJITter:TABLe:MGRaph) to occupy the space of all the grids (ON) or return to the display of tables in a grid (OFF).