:MEASure:PJITter:TABLe:MGRaph
Command Syntax
:MEASure:PJITterN:TABLe:MGRaph {J3U | J4U | J5U | J6U | J8U | JRMS | EOJ}
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Query Syntax
:MEASure:PJITterN:TABLe:MGRaph?
Description
This command selects the table that should be maximized in the PAM Jitter window area when using the :MEASure:PJITter:TABLe:DMAXimized command:
J3U— J3uJ4U— J4uJ5U— J5uJ6U— J6uJ8U— J8uJRMS— JrmsEOJ— EOJ (Even-Odd Jitter)