:MEASure:PJITter:TABLe:GSIZe
Command Syntax
:MEASure:PJITterN:TABLe:GSIZe {SMALl | MEDium | LARGe | OGRaph | OBTWo
| TBONe | TWBTwo | TBTHree | TBTWo | THBThree}
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Query Syntax
:MEASure:PJITterN:TABLe:GSIZe?
Description
This command selects the table size option in the PAM Jitter results content window:
SMALl— Auto fit smallMEDium— Auto fit mediumLARGe— Auto fit largeOGRaph— One graphOBTWo— 1x2TBONe— 2x1TWBTwo— 2x2TBTHree— 2x3TBTWo— 3x2THBThree— 3x3