:MEASure:SNDRatio:LMEans:SOURce
Command Syntax
:MEASure:SNDRatio:LMEans:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{N}— Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 isCHANnel4_2.DIFF{N}— Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) isDIFF5_3.CMODe{N}— Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) isCMODe5_3.FUNCtion{1:64}WMEMory{1:8}CGMemory{1:8}
Query Syntax
:MEASure:SNDRatio:LMEans:SOURce?
Description
Selects the source waveform on which to perform the :MEASure:SNDRatio:LMEans measurement. The source must be a displayed single-valued waveform.