:MEASure:VERTical:CPOWer

Command Syntax

:MEASure:VERTical:CPOWer

Query Syntax

:MEASure:VERTical:CPOWer?

Description

Moves the Carrier Power measurement to the top of the Results table or displays the measurement if it is not already shown on the table. The query form of the command returns the measured value.

Carrier Power is a measure of the power of a carrier signal without modulation. The Carrier Power measurement is ACrms2/(reference impedance) to give Power which is then converted to dBm using 10 log (Power/0.001).

Use the :MEASure:VERTical:CPOWer:SOURce command to specify the waveform to be measured.

Use :MEASure:TBASe:GENeral:METHod to change the definition of the waveform's top/base. Use :<waveform>:THReshold:GENeral:METHod to change the definition of the waveform's threshold.

Example Command Sequence

:MEASure:VERTical:CPOWer:SOURce CHAN1_1
:MEASure:VERTical:CPOWer
:MEASure:VERTical:CPOWer?

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Infiniium.query(':MEASure:VERTical:CPOWer:STATus?')):
	measurement = Infiniium.query(':MEASure:VERTical:CPOWer?')

If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Infiniium.query(':MEASure:VERTical:CPOWer:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
	measurement = Infiniium.query(':MEASure:VERTical:CPOWer?')

You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Querying Measurement Results and Statistics

You can query measurement results using the :MEASure:VERTical:CPOWer? query after making the proper instance settings.

If a measurement is installed into Results table (using the :MEASure:VERTical:CPOWer command) and you have made the proper instance settings, you can query statistics using common child queries.

Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.