:MEASure:VERTical:CPOWer:RIMPedance
Command Syntax
:MEASure:VERTical:CPOWer:RIMPedance <ohms>
<ohms> is an integer from 10 to 200.
Query Syntax
:MEASure:VERTical:CPOWer:RIMPedance?
Description
When the Auto Reference Impedance is off (see :MEASure:VERTical:CPOWer:AIMPedance), use this command to specify the reference impedance value.
When the Auto Reference Impedance is on, you can use the query to find the reference impedance value that has been automatically set.