:MEASure:VERTical:CPOWer:AIMPedance
Command Syntax
:MEASure:VERTical:CPOWer:AIMPedance {ON | OFF | 1 | 0}
Query Syntax
:MEASure:VERTical:CPOWer:AIMPedance?
Query Response
{1 | 0}
Description
For the Carrier Power measurement (see :MEASure:VERTical:CPOWer), this command turns on or off the Auto Reference Impedance. When off, you can specify the reference impedance with the :MEASure:VERTical:CPOWer:RIMPedance command.