Waveform Histogram Commands
Use the following commands to query the results that are shown in the W-Hist Stats content window.
- :MEASure:HISTogram{N}:HITS? (Total hits)
- :MEASure:HISTogram{N}:M1S? (% points within 1 standard deviation)
- :MEASure:HISTogram{N}:M2S? (% points within 2 standard deviation)
- :MEASure:HISTogram{N}:M3S? (% points within 3 standard deviation)
- :MEASure:HISTogram{N}:MAXimum? (Maximum)
- :MEASure:HISTogram{N}:MEAN? (Mean)
- :MEASure:HISTogram{N}:MEDian? (Median)
- :MEASure:HISTogram{N}:MINimum? (Minimum)
- :MEASure:HISTogram{N}:MODE? (Mode)
- :MEASure:HISTogram{N}:PEAK? (Peak hits)
- :MEASure:HISTogram{N}:PP? (Peak-to-peak hits)
- :MEASure:HISTogram{N}:SCALe? (Hits / display graticule)
- :MEASure:HISTogram{N}:STDDev? (Standard deviation)