:MTESt:ALIGnment:X

Command Syntax

:MTEStN:ALIGnment:X {AUTomatic | MANual}

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Query Syntax

:MTEStN:ALIGnment:X?

Description

Selects automatic or manual horizontal alignment of the selected mask to the eye diagram. If MANual is selected, use the following commands to scale the mask:

Child Commands