:MTESt:YTRack
Command Syntax
:MTEStN:YTRack {ON | OFF | 1 | 0}
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.
Query Syntax
:MTEStN:YTRack?
Query Response
{1 | 0}
Description
Turns logic-level tracking on or off, which affects the masks Y-axis scaling and position. Use the :MTESt:Y command to adjust logic-level one. Use the :MTESt:Y command to adjust logic-level zero.
- ON
- Logic level tracking is enabled and the logic levels track each other, allowing you to manually move the mask up and down on the display. For example, if you adjust the logic 1 level by 5 mW, the logic 0 level will also move by 5 mW.
- OFF
- You can independently scale the mask to logic level one and zero.