:NAVigation:EXIT

Command Syntax

:NAVigation:EXIT
            

Description

This command disables and exits navigation.

Clearing the display (:ACQuire:CDISplay) or making another acquisition, for example with a Run (:ACQuire:RUN) or Single (:ACQuire:SINGle), also exits navigation.

When exiting navigation, the acquisition state and waveform window scaling return to the values present when navigation was enabled. (The commands that enable navigation depend on the :NAVigation:SOURce?.)