:NAVigation:INDex

Command Syntax

:NAVigation:INDex <item_number>
            

Where <item_number> is an integer.

Query Syntax

:NAVigation:INDex?

Description

When navigation is enabled (see :NAVigation:IPRogress?), this command navigates to the item number specified.

The query returns the number of the item that has been navigated to. Zero is returned when navigation is not enabled.

You can also use the :NAVigation:FIRSt, :NAVigation:PREVious, :NAVigation:NEXT, or :NAVigation:LAST commands to navigate.