:NAVigation:IPRogress?
Query Syntax
:NAVigation:IPRogress?
Query Response
{0 | 1}
Description
This command returns whether navigation is enabled. "0" is No, and "1" is Yes.
The commands that enable navigation depend on the :NAVigation:SOURce?.