:NETWorks:TRACe:EYE:CCOunt
Command Syntax
:NETWorks:TRACeN:EYE:CCOunt <num_hits>
(missing or bad snippet)<num_hits> is an integer.
Query Syntax
:NETWorks:TRACeN:EYE:CCOunt?Description
This command specifies the minimum highest hit count in the real-time eye's color grade - gray scale database that must occur before making measurements on the data. Increasing this value lets more waveforms be collected before making measurements, thereby increasing measurement accuracy. The default value for this control is 1.