:NETWorks:TRACe:EYE:WINDow:WIDTh
Command Syntax
:NETWorks:TRACeN:EYE:WINDow:WIDTh<percent>
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
<percent> is a double.
Query Syntax
:NETWorks:TRACeN:EYE:WINDow:WIDTh?
Description
When the "At Clock Time" eye window determination method is selected (see :NETWorks:TRACe:EYE:WINDow:METHod), this command specifies the UI percentage width about the recovered clock location to use as the eye window. A zero percent for this setting means only the recovered clock location is used.
This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.