:NETWorks:TRACe:EYE:WINDow:TRACking
Command Syntax
:NETWorks:TRACeN:EYE:WINDow:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Syntax
:NETWorks:TRACeN:EYE:WINDow:TRACking?
Query Response
{1 | 0}
Description
Specifies whether a signal tracks the global eye window definition or uses its own eye window definition.
The global eye window definition is set using the :MEASure:EYE:WINDow commands (see Eye Window Configuration Commands).
Example Command Sequence
:NETWorks:TRACe2:EYE:WINDow:TRACking OFF :NETWorks:TRACe2:EYE:WINDow:METHod EOPening :NETWorks:TRACe2:EYE:WINDow:LEFT 40.0 :NETWorks:TRACe2:EYE:WINDow:RIGHt 60.0