:STATus:MESSage:EVENt?

Query Syntax

:STATus:MESSage:EVENt?

Description

Reads the message event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (MSG), which indicates if a message is displayed on Infiniium 2026's screen and placed in the message queue.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit 2 (MSG) of the Status Byte Register.

Message Register Commands
Register Read Write Command
Event ♦   :STATus:MESSage:EVENt?
Enable (mask) ♦ ♦ :STATus:MESSage:ENABle
Message Status Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — — — MSG
Enable
Register
                               
Sets to Bit 2 (MSG) of Status Byte Register

Bit Definitions

MSG
A true indicates that a message is displayed on Infiniium 2026's screen and placed in the message queue.