:STATus:USER:ENABle

Command Syntax

:STATus:USER:ENABle <mask>

<mask> is an integer, 0 to 65535, representing a mask for the bits in the event register.

Query Syntax

:STATus:USER:ENABle?

Description

Enters a decimal-weighted value in the user enable register that masks the ability to report bits in the user event register.

User Register Commands
Register Read Write Command
Event ♦   :STATus:USER:EVENt?
Enable (mask) ♦ ♦ :STATus:USER:ENABle
User Status Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — CONNection4 CONNection2 CONNection3 CONNection1 LCL
Enable
Register
                               
Sets to Bit 1 (USR) of Status Byte Register

Bit Definitions

LCL
A true indicates that Infiniium 2026 has transitioned from remote mode to local mode. This status bit originates from the local event register.
CONNection1
Reserved for future use.
CONNection3
Reserved for future use.
CONNection2
Reserved for future use.
CONNection4
Reserved for future use.