:TRIGger:RUNT:SOURce
Command Syntax
:TRIGger:RUNT:SOURce <trigger_source>
Where <trigger_source> can be:
CHANnel{N}— Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 isCHANnel4_2.
Query Syntax
:TRIGger:RUNT:SOURce?
Description
In the Runt trigger mode (see :TRIGger:MODE), this command selects the Source. You can choose from one of the analog input channels.