:TRIGger:SEQuence:SHOLd:CSOurce:EDGE

Command Syntax

:TRIGger:SEQuence{A|B}:SHOLd:CSOurce:EDGE  {POSitive | NEGative}

Query Syntax

:TRIGger:SEQuence{A|B}:SHOLd:CSOurce:EDGE?

Description

In the Setup And Hold trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the edge of the Clock Source (see :TRIGger:SEQuence:SHOLd:DSOurce) that will trigger.