:TRIGger:SEQuence:SHOLd:HTIMe
Command Syntax
:TRIGger:SEQuence{A|B}:SHOLd:HTIMe <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:SEQuence{A|B}:SHOLd:HTIMe?
Description
In the Setup And Hold trigger mode (see :TRIGger:SEQuence:MODE), when the trigger condition looks for hold time violations (see :TRIGger:SEQuence:SHOLd:MODE), this command specifies the minimum hold time.