:TRIGger:SEQuence:SHOLd:STIMe

Command Syntax

:TRIGger:SEQuence{A|B}:SHOLd:STIMe <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:SHOLd:STIMe?

Description

In the Setup And Hold trigger mode (see :TRIGger:SEQuence:MODE), when the trigger condition looks for setup time violations (see :TRIGger:SEQuence:SHOLd:MODE),, this command specifies the minimum setup time.