:TRIGger:SHOLd:HTIMe

Command Syntax

:TRIGger:SHOLd:HTIMe <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SHOLd:HTIMe?

Description

In the Setup And Hold trigger mode (see :TRIGger:MODE), when the trigger condition looks for hold time violations (see :TRIGger:SHOLd:MODE), this command specifies the minimum hold time.