:TRIGger:SHOLd:CSOurce
Command Syntax
:TRIGger:SHOLd:CSOurce <data_source>
Where <data_source> can be:
CHANnel{N}— Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 isCHANnel4_2.
Query Syntax
:TRIGger:SHOLd:CSOurce?
Description
In the Setup And Hold trigger mode (see :TRIGger:MODE), this command selects the Data Source. You can choose from one of the analog input channels.