:TRIGger:TIMeout:SOURce

Command Syntax

:TRIGger:TIMeout:SOURce  <trigger_source>

Where <trigger_source> can be:

  • CHANnel{N} — Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:TRIGger:TIMeout:SOURce?

Description

In the Timeout trigger mode (see :TRIGger:MODE), this command selects the Source. You can choose from one of the analog input channels.