:WAVeform:STATus:DETails?
Query Syntax
:WAVeform:STATus:DETails?
Description
Returns a string that may provide additional details for a questionable or invalid status. If the status is correct, a null string is returned.
For a basic description of a questionable or invalid status, use the :WAVeform:STATus:REASon? sibling query. Use the :WAVeform:STATus? parent query to determine if the decode is questionable or invalid.