:WAVeform:STATus?
Query Syntax
:WAVeform:STATus?
Description
Queries the status of the waveform data and returns the strings shown in the following table. Use the :WAVeform:STATus:REASon? child query to return a string that indicates why the data is invalid or questionable.
| Response | Description |
|---|---|
| CORR | The waveform data is correct. |
| INV | The waveform data is invalid. |
| QUES | The waveform data is questionable. |
Query the data using one of the following commands:
- :WAVeform:YFORmat:ASCii:YDATa?
- :WAVeform:YFORmat:DOUBle:YDATa?
- :WAVeform:YFORmat:FLOat:YDATa?
- :WAVeform:YFORmat:WORD:YDATa?
- :WAVeform:XYFormat:ASCii:YDATa?
- :WAVeform:XYFormat:ASCii:XDATa?
- :WAVeform:XYFormat:DOUBle:YDATa?
- :WAVeform:XYFormat:DOUBle:XDATa?
- :WAVeform:XYFormat:FLOat:YDATa?
- :WAVeform:XYFormat:FLOat:XDATa?