:WAVeform:CLIPped?
Query Syntax
:WAVeform:CLIPped?
Query Response
{NONE | CHIG | CLOW | CBOT}
NONE— No clippedCHIGh— Clipped highCLOW— Clipped lowCBOTh— Clipped high and low
Description
Returns whether the waveform data has been vertically clipped. The amplitude of a clipped-high data point is too high to be displayed on the screen. The amplitude of a clipped-low data point is too low to be displayed on the screen.
Clipped data points (high and low) have the value NaN (9.91E+37).
Use the :SYSTem:AUToscale command to properly scale the waveform to the display.
Use :WAVeform:SOURce to select the source waveform.