Bits Versus Symbols

In computer science the amount of information is measured in symbols (or bytes). Consequently, symbols/second units are used for the speed of information being transmitted. Digital communication codes information into physical properties. This coding is called modulation and packs one or multiple bits into symbols and then transmits each symbol separately. Therefore the speed of transmission is called the symbol rate and measured in baud. Symbol rate is also referred to as signaling rate, modulation rate, or baud rate. The inverse of the symbol rate is called the Unit Interval (UI). One UI is the nominal time to transmit one symbol:

UI = 1 / symbol rate

The traditional NRZ and RZ modulations code use one bit per symbol, and the baud rate happens to be the same number as the symbol rate. Consequently, people used baud and symbols/s interchangeable although technically they are not the same. More advanced modulation techniques code more than one bit into each symbol. For example, PAM4 codes two bits into each symbol. In such cases, the symbol rate is twice the baud rate:

Symbol Rate = Signaling Rate * log2 (Nvalues)

Where Nvalues is the number of allowed physical values

For example, a 25.78 Gbaud PAM4 signal transmits 51.56 Gbits/s. Each unit interval is 38.79 ps long and the nominal amplitude in the center is exactly one out of 4 possible choices. Some RF signals use complex modulations such as QAM-16. In this case each symbol contains one out of 16 possible complex values and the symbol rate is four times the baud rate.

Examples of Signal Parameters Combinations for NRZ and PAM4 Signals
Signal Parameters NRZ PAM4
Example 1 Example 2 Example 3 Example 1 Example 2 Example 3
Bits/Symbol 1 1 1 2 2 2
Signaling Rate 25 GBd 28 GBd 56 GBd 25 GBd 28 GBd 56 GBd
Unit Interval 40 ps 36 ps 18 ps 40 ps 36 ps 18 ps
Symbol Rate 25 GBd 28 GBd 56 GBd 50 GBd 56 GBd 112 GBd
Fundamental Frequency 13 GHz 14 GHz 28 GHz 13 GHz 14 GHz 28 GHz
3rd Harmonic 38 GHz 42 GHz 84 GHz 38 GHz 42 GHz 84 GHz
NRZ Waveform
PAM4 Waveform