Pattern Length
To measure Pattern Length, Clock Recovery must be performed to determine the edge locations.
The Pattern Length measurement looks for at least two error-free copies of an identical repeating bit pattern in acquisition memory. If a repeating bit pattern is found, its length is reported in the measurement results.
Configurable Measurement Parameters
This measurement is affected by the following settings (choose Measure > Thresholds...):
- Thresholds tab
To measure
- Click the toolbar's Data tab.
-
If necessary, click the toolbar's More buttons to locate the Pattern Length button.
- Click the button.
- Select the signal on which to make the measurement.
- Click Apply.
SCPI Command
:MEASure:DATA:PLENgth