Thresholds
Within the Thresholds tab of the Configure Measurements dialog box, there are these subtabs:
- General — for everything except rise/fall time measurements. See General Thresholds.
- Rise/Fall — for rise and fall time measurements. See Rise/Fall Thresholds.
- PAM3 General — for everything except rise/fall time measurements. See PAM3 General Thresholds.
- PAM3 Rise/Fall — for rise and fall time measurements. See PAM3 Rise/Fall Thresholds.
- PAM4 General — for everything except rise/fall time measurements. See PAM4 General Thresholds.
- PAM4 Rise/Fall — for rise and fall time measurements. See PAM4 Rise/Fall Thresholds.