Getting Started

To view a signal on the oscilloscope

  1. Press the [Default Setup] key on the oscilloscope's front panel. A Default Setup configures the instrument in a known startup condition including:
    • Edge triggering. To learn more about triggering, see Trigger Setup.
    • Displays Channel 1 on the lowest numbered occupied connection for display. All other channel inputs turned off.
  2. Connect a signal to a front-panel channel input. In this example, the signal is connected to Channel 1, since Default Setup will automatically select Channel 1. Channel inputs are located on the front-panel of the real-time oscilloscope.
  3. Press the oscilloscope's front panel [Auto Scale] key.

The oscilloscope's graphical user interface is known as Infiniium, and it is important to understand the different ways in which the oscilloscope and Infiniium can be used.

For optimum measurement results, allow the temperature of the instrument to stabilize after applying power.