Symbol Rates
The following table lists the standard waveform symbol rates selections available from any of the following controls:
This list includes the rate designation for the filter associated with the symbol rate (SONET/SDH, Fibre Channel, or Gigabit Ethernet).
| Symbol Rate in Baud | Designation |
|---|---|
| 51.84 MBd | STM-0/OC-1 |
| 125.0 MBd | FDDI/100M Ethernet |
| 155.52 MBd | STM-1/OC-3 |
| 270.0 MBd | SDI |
| 614.4 MBd | CPRI |
| 622.08 MBd | STM-4/OC-12 |
| 768.00 MBd | OBSAI |
| 1.06250 GBd | FC-1063 |
| 1.22880 GBd | CPRI 2x |
| 1.244160 GBd | GPON/OC-24 |
| 1.25000 GBd | Gb Ethernet |
| 1.48500 GBd | SDI |
| 1.50000 GBd | SATA-1/SAS-1 |
| 1.53600 GBd | OBSAI 2x |
| 2.12500 GBd | FC-2125 (2x) |
| 2.4576 GBd | CPRI 4x |
| 2.48832 GBd | STM-16/OC-48 |
| 2.50000 GBd | PCIe1/2 Gb Ethernet/InfiniBand |
| 2.6660570 GBd | STM-16/OC-48 FEC |
| 2.97000 GBd | SDI |
| 3.00000 GBd | SATA-2/SAS-2 |
| 3.07200 GBd | CPRI 5x / OBSAI 4x |
| 3.12500 GBd | XAUI / 10GbE Base-LX4 |
| 3.18750 GBd | FC-3187/10GBE Base-LX4 |
| 3.25000 GBd | Rapid IO |
| 3.32000 GBd | 12x Parallel Optics |
| 4.25000 GBd | 4x Fibre Channel |
| 4.9152 GBd | CPRI 8x |
| 5.00000GBd | PCIe-2/2x InfiniBand |
| 6.00000 GBd | SATA-3/SAS3/CEI |
| 6.144 GBd | CPRI 10X / OBSAI 8X |
| 6.25000 GBd | 2x XAUI |
| 6.37500 GBd | CEI 6G+ |
| 8.00000 GBd | PCIe-3 |
| 8.50000 GBd | 8x Fibre Channel |
| 9.8304 GBd | CPRI 16x |
| 9.95328 GBd | STM-64/OC-192/10GbEthernet |
| 10.00 GBd | InfiniBand QDR |
| 10.1376 GBd | CPRI 20x |
| 10.3125 GBd | 10Gb Ethernet LR/ER |
| 10.51875 GBd | 10GFC |
| 10.664230 GBd | STM-64/OC-192 FEC |
| 10.7090 GBd | STM-64/OC-192 FEC |
| 11.0000 GBd | CEI 11G |
| 11.0957 GBd | 10Gb Ethernet FEC |
| 11.3170 GBd | 10GFC FEC |
| 12.249450 GBd | STM-64/OC-192 SuperFEC |
| 12.44160000 GBd | ITU-T PON |
| 14.025000 GBd | 16x Fibre Channel |
| 14.06250 GBd | InfiniBand FDR |
| 16.00000 GBd | PCIe-4 |
| 24.33024000 GBd | CPRI 48x |
| 24.88320000 GBd | ITU-T PON |
| 25.78125 GBd | 100Gb Ethernet / 4 / InfiniBand EDR |
| 26.56250000 GBd | 400GBASE-SR16 |
| 27.7393 GBd | 100Gb Ethernet / 4 FEC |
| 27.952493 GBd | OTU4/ITU-T G.959.1 |
| 28.05 GBd | 32x Fibre Channel |
| 28.9 GBd | 64G Fibre Channel |
| 32.00000 GBd | PCIe-5/PCIe-6 |
| 39.81312 GBd | STM-256/OC-768 |
| 41.250000 GBd | 40Gb Ethernet |
| 43.018413 GBd | STM-256/OC-768 FEC |
| 49.76640000 GBd | ITU-T PON |
| 53.125 GBd | 400GBASE |
| 79.62624 GBd | STM-512/OC-1536 |
| 159.25248 GBd | STM-1024/OC-3072 |