Executing Load Calibration

Use the following procedure to perform Load calibration using the 7-mm calibration kit using Wizard.

  1. Press Cal Wizard to display the Calibration Wizard.

  2. Execute Open calibration.

  3. Execute Short calibration.

  4. Execute Low-Loss Capacitor calibration.

  1. Remove the Low-Loss Capacitor standard from the 7-mm connector of the test head installed on the test fixture stand.

  2. Spin the knurled nut of the 7-mm connector of the test head installed on the test fixture stand to be protruded to its full extent at the top.

  3. Place the Load standard on the 7-mm connector of the test head installed on the test fixture stand and turn the Load standard clockwise until snug using the torque wrench.

  4. Click Load to perform the Load calibration.

  5. Click Save to finish the calibration.