:CALCulate:COMParator:DATA:RDC?
Returns the most recent Rdc limit evaluation result when the Rdc measurement feature and the comparator feature are enabled (Query only).
|
Parameter |
State |
|
Description |
O/1 that indicates Rdc beyond or within limit |
|
Range |
Select from the following:
|
|
Preset value |
If either the Rdc measurement feature or the comparator feature is disabled, the command returns the previous sorting result. However, the command reĀturns zero if the E4982A has been reset or the Rdc limit evaluation has not been executed since turning ON the E4982A. |
No equivalent keys are available on the front panel.