Other topics about Specifying Measurement Conditions
You can instruct the instrument to show or hide the entire set of measurement results, which includes the measurement results for measurement parameters 1 through 4, test signal level monitoring, and Rdc measurement. To do so, use the following command:
You can set the following display attributes for each value:
Number of digits
Whether to fix the decimal point
Most significant digit when the value is displayed with the decimal point fixed
Whether to show or hide the value
To set the above display attributes, use the commands listed in the table below.
|
|
Results for measurement parameters :CALC1:parameter 1 :CALC2:parameter 2 :CALC3:parameter 3 :CALC4:paramter 4 |
Results of test signal level monitoring :CALC11:current level :CALC12:voltage level |
Result of Rdc measurement |
|
Number of digits |
|||
|
Whether to fix decimal point |
|||
|
Most significant digit when decimal point is fixed |
|||
|
Whether to show or hide value |
*1. This command not only sets whether to show or hide the result of Rdc measurement but also whether to turn ON or OFF the Rdc measurement function. You cannot use the command to only show or hide the Rdc result.
To define each of the seven display items (:LAB1 through :LAB7) that appear on the list measurement screen, use the following command:
You can instruct the instrument to show or hide all of the displayed items except the menu bar by using the following command:
You can instruct the instrument to turn ON or OFF the backlight of the LCD screen by using the following command:
If the backlight is OFF, you cannot read displayed information on the screen.
To choose whether to show or hide the title display area (the topmost area on the screen), use the following command:
To define the title string that appears in the title display area, use the following command:
To choose whether to show or hide the current date and time in the extreme right of the status display area, use the following command:
Also, you can choose whether to automatically update the time display in increments of 1 minute as time elapses or keep the day, hour and minute set to the date/time when you turned on the display. To make this selection, use the following command: