Window for displaying the traces. Because a channel corresponds to a window, it is called a channel window. When the outer frame of a channel window is displayed in light gray, it shows that the channel is an active channel (the channel for which setup is being performed). In the following figure, Channel 1 (the upper window) is the active channel.
Channel 1 Window and Channel 2 Window describes different measurement parameters available in the channel measurement window. The measurement parameters described in the Channel 1 and 2 Window correspond to the same channel measurement window and are displayed in separate windows for ease of read.
Displays the averaging factor and averaging count when averaging is turned on.
|
n/m (displayed in blue) |
Averaging: ON (m: averaging factor; n: averaging count) |
|
(not displayed) |
Averaging: OFF |
It shows the bandwidth data for a trace when the bandwidth function is turned on.
|
|
Correction Point:Fixed Freq |
Correction Point:User Freq |
|
User Correction: On |
COR |
Cor (Neither interpolation nor extrapolation is being executed.) |
|
|
C? (Interpolation is being executed.) |
|
|
User Correction: Off |
None |
|
|
Status |
Indicator display |
|||
|
Open |
Short |
Load |
||
|
Off |
Off |
Off |
None |
None |
|
On |
Off |
Off |
Comp O |
COMP O |
|
Off |
On |
Off |
Comp S |
COMP S |
|
Off |
Off |
On |
Comp L |
COMP L |
|
On |
On |
Off |
Comp OS |
COMP OS |
|
On |
Off |
On |
Comp OL |
COMP OL |
|
Off |
On |
On |
Comp SL |
COMP SL |
|
On |
On |
On |
Comp OSL |
COMP OSL |
When the span is narrowed from the span of compensation in "user point", ? is displayed after COMP, like COMP? OSL.
PEXT or PExt is displayed when Port Extension is turned on and Length or Time is not zero.
PEXT: Fixed point
PExt: User point
Indicates the channel number. To make a channel active, use Channel Next or Channel Prev. Clicking inside a channel window will also make the channel active.
Displays the update status of traces on the channel.
|
! |
Measurement in progress. When the sweep time exceeds 1.5 seconds, ↑ is displayed at the point on the trace. |
|
# |
Invalid traces. The measurement conditions have changed, but the traces on the channel currently displayed have not been updated to match the new conditions. |
|
(No display) |
The measurement has not been executed. |
You can assign a title to each channel and have the title displayed on the bar.
DC Monitor values are displayed when the DC monitor function is turned on.
Equivalent Circuit Model/Simulation Result are displayed for the equivalent circuit.
Y-axis divisions in the rectangular display format. When traces in the rectangular display format are overlaid, the Y-axis divisions for the active trace are displayed. The value of the reference line (the division line between
and
) is entered numerically by opening the data entry bar using the keys: Scale > Reference Value. You can change values of the reference line at one-division intervals by placing the mouse pointer in the area of the graticule label (the pointer changes from
to
), moving the pointer vertically with the left mouse button pressed, and then releasing the button at the desired location.
Indicates the positions of markers on the stimulus axis.
|
|
Active marker indicator |
|
|
Non-active marker indicator |
You can also move a marker to the desired position by placing the mouse pointer on the marker indicator or position of the marker itself (the pointer changes from
to
), moving the indicator vertically with the left mouse button pressed, and then releasing the button at the desired location.
Displayed marker number is listed. For the active marker (the one for which setup and analysis are being performed), > is displayed at the left of the marker number. For the reference marker,
is displayed instead of the marker number.
The marker stimulus and response values for each marker is displayed here. Two (or three) response values are displayed for data in Smith chart or polar display format.
The markers used for reading values on a trace. Up to 10 markers can be displayed for each trace.
|
|
Active marker (the one for which setup and analysis are being performed). |
|
|
Non-active marker. |
Here, "n" denotes a marker number. For the reference marker, however, nothing is displayed at the location of n. Clicking the marker or one of the Marker Indicators makes the marker active.
It shows the statistics data for a trace (span, mean, standard deviation, and peak-to-peak) when the statistic function is turned on.
Measurement parameters are displayed.
Indicates the OSC level, DC Bias and CW frequency in the following conditions.
|
Indicator type |
Sweep type |
|
OSC level |
Frequency (Liner/Log) and DC Biasl |
|
DC Bias (when DC bias is ON) |
Frequency (Liner/Log) and OSC level |
|
CW frequency |
OSC level and DC Bias |
The indicators that indicate the position of the reference line for the Y-axis scale in the rectangular display format. One indicator is to the right and the other is to the left of the scale (
and
). To enter a numeric value for the position of the reference line, open the data entry bar using the keys: Scale > Reference Position. You can also move the position of the reference line by placing the mouse pointer on either of the two reference line indicators (the pointer changes from
to
.), moving the indicator vertically with the left mouse button kept pressed, and then releasing the button at the desired location (i.e., a drag-and-drop operation).
The scale for each trace is displayed here.
When Linear scale is selected at Y-Axis
The scale/Div and Reference values are displayed.
This example shows that "50.00°" corresponds to 50° per division. "Ref 0.000°" shows that the value of the reference line is 0°.
When Log scale is selected at Y-Axis
The top and bottom values of Y-Axis are displayed.
Indicates the sweep range by using the start/stop or center/span.
The names of the traces, such as Tr1, on the channel are displayed here. The symbol
at the right of the trace name indicates the active trace (the trace for which setup is being performed).
To make a trace active, use Trace Next or Trace Prev. Clicking the line where the trace name is placed (the mouse pointer changes from
to
) also makes a trace active.
In the rectangular display format, the trace number is displayed in the same color as the trace at the right end of each trace.
The setup for each trace is displayed here.
Trace status display
|
Classification |
Contents inside [ ] |
Meaning |
|
Memory traces |
Nothing |
Data trace: ON, Memory trace: OFF |
|
|
M |
Data trace: OFF, Memory trace: ON |
|
|
D&M |
Data trace: ON, Memory trace: ON |
|
|
off |
Data trace: OFF, Memory trace: OFF |
|
Performing data math |
D+M (D+M&M) |
Execution of Data+Mem math |
|
When a memory trace is ON, see the contents inside () |
D-M (D-M&M) |
Execution of Data-Mem math |
|
|
D*M (D*M&M) |
Execution of Data*Mem math |
|
|
D/M (D/M&M) |
Execution of Data/Mem math |
|
Equation Editor |
Equ |
Equation Editor: ON |