Other topics about Transient Measurement
The transient measurement has two measurement modes: Wide-Narrow band mode, which consists of four traces of wide and narrow, and Narrow-Narrow band mode, which consists of six traces of narrow and narrow. For more information, refer to Overall Instrument Operation. Also refer to External Reference Signal Input Port.
You can change the measurement mode from Wide-Narrow to Narrow-Narrow mode or vice-versa. In each measurement layout, data will be assigned as measurement layout. In the Wide-Narrow mode, the upper-left is wide-band frequency, the upper-right is narrow-band frequency, the lower-left is narrow-band power and the lower-right is narrow-band phase.
This function is added since firmware rev. A.03.20.
You can select either Wide-Narrow or Narrow-Narrow by pressing the Setup > Measurement Mode key. Wide-Narrow mode is selected by default.
Measurement layout

Displays off trace 6 to 8 when Wide-Narrow measurement, display off trace 1 when Narrow-Narrow measurement.
Trace 5 is always OFF.
You can select the measurement window when Narrow-Narrow measurement mode is selected.
Press Display > Parameters.
Select the measurement window from the softkey menu list. The available measurement windows are as follows. All is selected by default.
Measurement Window List
|
Softkey |
Overview |
|
All |
Displays all traces. |
|
Frequency |
Displays narrow band frequency by bisecting the screen vertically, with channel 1 displayed above channel 2. |
|
Power |
Displays narrow band power by bisecting the screen vertically, with channel 1 displayed above channel 2. |
|
Phase |
Displays narrow band phase by bisecting the screen vertically, with channel 1 displayed above channel 2. |
Trace Layout