Sets and reads the VNA Preferences settings.
SYSTem:PREFerences | DEFault | ITEM | ASMRamp | CORRectrion | PARallel | PROCess | CSET | COMPact | DIALog | SHOW | LICense | FIXTure | CIRCuit | DEFAults | GDELay | LEGacy | TWOPoint | KEYS | MCMethod | MCPreset | MRU | OFFSet | RCV | SRC
| PSRTrace | QSTart | RECeivers | CERRor | REMote | AUTO | [:STATe] | ROSCillator | RECall | RTOF | USOLt SOURce | GLOBal | MODulation | FILE? | LOAD | [:STATe] | OUTPut | [:STATe] | POFF | IGNore | [:STATe] | POWer | [:STATe]
|
Click on a keyword to view the command details.
See Also
Example Programs
Applicable Models: E505xA (Read-Write) Set and return whether ramp sweep is used whenever possible when sweep mode is in Auto. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable ramp sweep. OFF (0) Disable ramp sweep. |
Examples |
SYST:PREF:ITEM:ASMR
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:ASMRamp? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Write-only) Resets the VNA preferences to their default settings. Some default settings vary depending on the VNA Model. Learn more about VNA Preferences. |
|
Examples |
SYST:PREF:DEF |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Enable or disable parallel processing in the CPU which provides higher calculation speeds. |
|
Parameters |
|
<bool> |
Choose from: OFF (0) Disable parallel processing. ON (1) Enable parallel processing. |
Examples |
SYST:PREF:ITEM:CORR:PAR:PROC
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:CORRection:PARallel:PROCess? |
Return Type |
Boolean |
ON or 1 |
|
Applicable Models: All (Read-Write) Set and return whether External Devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<bool> |
Choose from: OFF (0) External devices remain active when the VNA is Preset or when a Instrument State is recalled. ON (1) External devices are de-activated (SYST:CONF:EDEV:STAT to OFF) when the VNA is Preset or when a Instrument State is recalled. |
Examples |
SYST:PREF:ITEM:EDEV:DPOL
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:EDEV:DPOLicy? |
Return Type |
Boolean |
ON or 1 |
|
Applicable Models: All (Read-Write) Enables/disables the creation of compact calsets. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable creation of compact calsets. OFF (0) Disable creation of compact calsets. |
Examples |
SYST:PREF:ITEM:CSET:COMP 1 system:preferences:item:cset:compact OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:CSET:COMPact? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Enables/disables showing the licensed features dialog on startup. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable showing licensed features on startup. OFF (0) Disable showing licensed features on startup. |
Examples |
SYST:PREF:ITEM:DIAL:SHOW:LIC
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:DIALog:SHOW:LICense? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Sets whether a Swept IMD or IMDx calibration can exceed the stop frequency limit of an ECal module. Learn more. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Allow extrapolation. OFF (0) Do NOT allow extrapolation. |
Examples |
SYST:PREF:ITEM:EEXT 1 system:preferences:item:eextrapolate OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:EEXTrapolate? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Sets the Series-C and Shunt-L components to legacy or theoretical behavior when set to zero. Note: This command is only applicable in Firmware versions A.14.00.00 and later. |
|
Parameters |
|
<char> |
Choose from: THEoretical- When "R" or "L" is set to 0, the component is defined as "Short"; when "C" or "G" is set to 0, the component is defined as "Open". LEGacy - Legacy operation provided as a user-convenience for backward compatibility. When either of the two components of Series-C, "C", and "G", is set to 0, the component is defined as "Open"; when both components are set to 0, they are defined as "Short". When either of the two components of Shunt-L, "L", and "R", is set to 0, the component is defined as "Short"; when both components are set to 0, they are defined as "Open". |
Examples |
SYST:PREF:ITEM:FIXT:CIRC:DEFA
THE |
Query Syntax |
SYSTem:PREFerences:ITEM:FIXTure:CIRCuit:DEFAults? |
Return Type |
Character |
THEoretical |
|
Applicable Models: All (Read-Write) Sets the group delay aperture to use the legacy computation method. Learn more about group delay aperture. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Use legacy computation method. OFF (0) Do not use legacy computation method. |
Examples |
SYST:PREF:ITEM:GDEL:LEG
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:GDELay:LEGacy? |
Return Type |
Boolean |
|
|
OFF |
Applicable Models: All (Read-Write) Sets the default group delay aperture setting. Learn more about group delay aperture. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Sets default group delay aperture to 2 points. OFF (0) Sets default group delay aperture to 11 points. |
Examples |
SYST:PREF:ITEM:GDELay:TWOPoint
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:GDELay:TWOPoint? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return whether the keys are displayed or not. |
|
Parameters |
|
<bool> |
Choose from: ON (1) – Turn keys on. OFF (0) – Turn keys off. |
Examples |
SYST:PREF:ITEM:KEYS 1 system:preferences:item:keys OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:KEYS? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: All (Read-Write) Sets the bandwidth search preference to start a bandwidth or notch search in either peak or marker mode. |
|
Parameters |
|
<char> |
Choose from: MARKer - BW/Notch marker search reference is set to current marker position after Preset. . PEAK - BW/Notch marker search reference is set to peak after Preset. |
Examples |
SYST:PREF:ITEM:MARK:BAND:SEAR
MARK |
Query Syntax |
SYSTem:PREFerences:ITEM:MARKer:BANDwidth:SEARch? |
Return Type |
Character |
MARK (E5080A/B), PEAK (Others) |
|
Applicable Models:All (Read-Write) Set and return whether to use one marker for marker search. Enabled behavior:
Disabled behavior:
|
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable single marker search. OFF (0) Disable single marker search. |
Examples |
SYST:PREF:ITEM:MARK:SING
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:MARKer:SINGle? |
Return Type |
Boolean |
ON |
|
Applicable Models: All (Read-Write) Set and return whether the Coupled Markers setting controls the ON|OFF state of markers that are coupled. Learn more about Coupled Markers. Refer also to CALC:MEAS:MARK:COUP:STATe ON. |
|
Parameters |
|
<bool> |
Choose from: ON (1) – With Coupled Markers ON, when a marker is turned on, the same-numbered marker on all coupled traces will also be turned on. Likewise, turning off a marker will turn it off on all coupled traces. OFF (0) – Turning a marker on or off will have no effect on the markers on other traces. |
Examples |
SYST:PREF:ITEM:MCC 1 system:preferences:item:mccontrol OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:MCControl? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: All (Read-Write) Set and return whether Coupled Markers is set to Channel or All after Preset. Learn more about Coupled Markers. Refer also to CALC:MEAS:MARK:COUP:STATe ON and SYST:PREF:ITEM:MCPR ON. |
|
Parameters |
|
<bool> |
Choose from: ON (1) – Marker Coupling Method is set to Channel after Preset. OFF (0) – Marker Coupling Method is set to ALL after Preset. |
Examples |
SYST:PREF:ITEM:MCM 1 system:preferences:item:mcmethod OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:MCMethod? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: All (Read-Write) Set and return whether Coupled Markers is set to ON or OFF after Preset. Learn more about Coupled Markers. |
|
Parameters |
|
<bool> |
Choose from: OFF (0) – Coupled Markers is OFF after Preset. ON (1) – Coupled Markers is ON after Preset. |
Examples |
SYST:PREF:ITEM:MCPR 1 system:preferences:item:mcpreset OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:MCPReset? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: N522xB, N523xB, N524xB, M983xA (Read-Write) Sets and reads the state of the memory data interpolation default preference. The PNA will return to the default interpolation state after a Preset, creating a new trace, or closing the PNA application. Learn more. |
|
Parameters |
|
<bool> |
Choose from: 0 - OFF - Set memory interpolation to OFF as the default. 1 - ON - Set memory interpolation to ON as the default. |
Examples |
SYST:PREF:ITEM:MINT 1 |
Query Syntax |
SYSTem:PREFerences:ITEM:MINTerpolate? |
Return Type |
Boolean |
0 |
|
Applicable Models: All (Read-Write) Set and return whether to list files for recall on softkeys by most-recently used or alphabetically. |
|
Parameters |
|
<bool> |
Choose from: ON (1) – Recall softkeys show most recently-used files. OFF (0) – Recall softkeys show alphabetically-ordered files. |
Examples |
SYST:PREF:ITEM:MRU 1 system:preferences:item:mru OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:MRU? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: All (Read-Write) Set and return whether to offset the test port receivers by the amount of receiver attenuation. Learn more. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Offset the test port receivers OFF (0) Do NOT offset the test port receivers |
Examples |
SYST:PREF:ITEM:OFFS:RCV
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:OFFSet:RCV? |
Return Type |
Boolean |
PNA-L and E836xB: OFF (does NOT offset the display). PNA-X: ON (offsets the display). |
|
Applicable Models: All (Read-Write) Set and return whether to offset the reference receiver by the amount of source attenuation. Learn more. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Offset the reference receivers. OFF (0) Do NOT Offset the reference receivers. |
Examples |
SYST:PREF:ITEM:OFFS:SRC
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:OFFSet:SRC? |
Return Type |
Boolean |
All models: ON (offset the display). |
|
Applicable Models: All (Read-Write) Display the power level measured by the ADC (IF Signal) at the bottom left of the screen in parentheses, in addition to the input power level which is measured at the detector. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Display the power level measured by the ADC (IF Signal) OFF (0) Do not display the power level measured by the ADC (IF Signal) |
Examples |
SYST:PREF:ITEM:PN:DISP:POW:IF:STAT
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:PN:DISPlay:POWer:IF[:STATe]? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return preset confirmation. If preset confirmation is OFF, pressing the green PRESET key presets the instrument and opens the Preset softkey menu. If preset confirmation is ON, pressing the green PRESET causes the Preset menu to appear. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable preset confirmation. OFF (0) Disable preset confirmation. |
Examples |
SYST:PREF:ITEM:PRES:CONF
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:PRESet:CONFirm? |
Return Type |
Boolean |
ON |
|
Applicable Models: All (Read-Write) Set and return the Preset Power ON/OFF state. Learn more. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<char> |
Choose from: ON - Instrument Preset always turns RF power ON. AUTO - When the current power setting is OFF, leave power OFF after Preset. When the current power setting is ON, turn power ON after Preset. |
Examples |
SYST:PREF:ITEM:PRE:POW
ON |
Query Syntax |
SYSTem:PREFerences:ITEM:PREset:POWer[:STATe]? |
Return Type |
Character |
ON |
|
Applicable Models: All (Read-Write) At the end of a power sweep, while waiting to trigger the next sweep, maintain source power at either the start power level or at the stop power level. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<char> |
Choose from: STARt - Maintain source power at the start power level. STOP - Maintain source power at the stop power level. |
Examples |
SYST:PREF:ITEM:PSRT
STOP |
Query Syntax |
SYSTem:PREFerences:ITEM:PSRTrace? |
Return Type |
Character |
STARt |
|
Applicable Models: All (Read-Write) This command controls the on/off state of the preference, "On PRESET show Quick Start dialog". |
|
Parameters |
|
<bool> |
Choose from: ON (1) Display the Quick Start dialog on PRESET. OFF (0) Do not display the Quick Start dialog on PRESET. |
Examples |
SYST:PREF:ITEM:QST
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:QST? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return whether to display receiver overload warnings. Learn more. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Display overload warnings, OFF (0) Do NOT display overload warnings. |
Examples |
SYST:PREF:ITEM:REC:CERR 1 system:preferences:item:receivers:cerror:state OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:RECeivers:CERRor[:STATe]? |
Return Type |
Boolean |
ON |
|
Applicable Models: All (Read-Write) Set and return whether to turn source power OFF when a receiver is overloaded. Learn more. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Turn OFF source power to ALL ports when a receiver is overloaded. OFF (0) Power remains ON when a receiver is overloaded. |
Examples |
SYST:PREF:ITEM:REC:OVER:POW 1 system:preferences:item:receivers:overload:power:state OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:RECeivers:OVERload:POWer[:STATe]? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA, M983xA (Read-Write) Set and return whether to draw limits lines in Red or the trace color. |
|
Parameters |
|
<bool> |
Choose from: ON (1) All Limit lines are drawn in Red. OFF (0) Limit lines are drawn the same color as the trace. |
Examples |
SYST:PREF:ITEM:REDL 1 system:preferences:item:redlimits OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:REDLimits? |
Return Type |
Boolean |
OFF |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA, M983xA (Read-Write) Set and return whether to treat marker 10 as a reference marker. If set to ON (1) for legacy behavior, marker 10 is the reference marker. If set to OFF (0), marker 16 is the reference marker and marker 10 becomes a normal marker. Learn more. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Marker 10 is always a reference marker (Pre A.10.40 behavior). OFF (0) Marker 10 is just another marker and marker 16 becomes the reference marker. See Reference Marker commands |
Examples |
SYST:PREF:ITEM:REFM 1 system:preferences:item:refmarker OFF |
Query Syntax |
SYSTem:PREFerences:ITEM:REFMarker? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Enables/disables changing from local to remote status when a SCPI command is received. |
|
Parameters |
|
<bool> |
Choose from: OFF (0) Turn OFF local/remote behavior. ON (1) Turn ON local/remote behavior. |
Examples |
SYST:PREF:ITEM:REM:AUTO
0 |
Query Syntax |
SYSTem:PREFerences:ITEM:REMote:AUTO[:STATe]? |
Return Type |
Boolean |
ON |
|
Applicable Models: N522xB, N523xB, N524xB, E5080B, E5081A (Read-Write) For single-band frequency or segment sweeps ONLY, specify whether to turn RF power ON or OFF during a retrace. Learn more about RF power during sweep retrace. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. This setting remains until changed using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<char> |
Choose from: AUTO: Power is left ON during retrace of single-band frequency or segment sweeps ONLY. OFF: Power is turned OFF during retrace of single-band frequency or segment sweeps ONLY. |
Examples |
SYST:PREF:ITEM:RETR:POW OFF system:preferences:item:retrace:power auto |
Query Syntax |
SYSTem:PREFerences:ITEM:RETRace:POWer? |
Return Type |
Character |
AUTO |
|
Applicable Models: All (Read-Write) Enables/disables External Reference settings being affected by Recall/Preset. |
|
Parameters |
|
<bool> |
Choose from: OFF (0) External Reference settings will be maintained until changed. ON (1) External Reference settings will be affected by Recall/Preset. |
Examples |
SYST:PREF:ITEM:ROSC:REC
0 |
Query Syntax |
SYSTem:PREFerences:ITEM:ROSCillator:RECall? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return whether to display limit line failures as red trace segments or red data points (dots). Learn more. |
|
Parameters |
|
<bool> |
Choose from: ON (1) Display failures as red trace segments. (Red Trace On Fail). OFF (0) Display failures as red data points (dots). |
Examples |
SYST:PREF:ITEM:RTOF
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:RTOF? |
Return Type |
Boolean |
OFF |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA, M983xA (Read-Write) This command controls the on/off state of the preference, "Use keyboard to navigate softkeys". |
|
Parameters |
|
<bool> |
Choose from: ON (1) Enable softkey navigation with keyboard. OFF (0) Disable softkey navigation with keyboard. |
Examples |
SYST:PREF:ITEM:SOFT:NAV
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:SOFTkeys:NAVigation? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Sets the default setting for the Noise Tuner switch. This is the setting that occurs when a new channel is created. Learn more. This command will return an error on VNA models with a built-in Noise tuner. To send this command using the VNA front panel, open the GPIB Command Processor Console, then type either of the following examples at the command prompt. Then type the Query Syntax and press enter to be sure the VNA took the command. This setting remains until changed using this command, or until the hard drive is changed or reformatted. |
|
Parameters |
|
<string> |
Name of the switch to set. Choose from:
|
<int> |
Value to set. Choose from: 0 Sets the default (preset) to INTERNAL 1 Sets the default (preset) to EXTERNAL |
Examples |
SYST:PREF:ITEM:SWIT:DEF "Port1NoiseTuner" 1 'Write system:preferences:item:switch:def? "Port1NoiseTuner" 'Read |
Query Syntax |
SYSTem:PREFerences:ITEM:SWITch:DEF? <switch> |
Return Type |
Integer |
1 (External) |
|
Applicable Models: All (Read-Write) This command controls the on/off state of the preference, "Use Unknown thru math for SOLT methods". |
|
Parameters |
|
<bool> |
Choose from: ON (1) Error terms are computed using the unknown thru method. OFF (0)Error terms are computed using the definition of the defined thru. |
Examples |
SYST:PREF:ITEM:USOL
1 |
Query Syntax |
SYSTem:PREFerences:ITEM:USOLt? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return the frequency of the specified global source. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<num> |
Global source frequency. Choose any number between the minimum and maximum frequency limits of the analyzer. Units are Hz. |
Examples |
SYST:PREF:SOUR:GLOB:FREQ 1E9 system:preferences:source2:global:frequency 1 GHz |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal:FREQuency? |
Return Type |
Numeric |
Not Applicable |
|
Applicable Models: All (Read only) Returns the filename of the currently loaded internal source modulation file. Learn more. |
|
Parameters |
None |
<port> |
Source port number of the VNA. |
Examples |
SYST:PREF:SOUR1:GLOB:MOD:FILE? |
Return Type |
String |
Not Applicable |
|
Applicable Models: All (Write-only) Loads the internal source modulation file. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<filename> |
Modulation file name. |
Examples |
SYST:PREF:SOUR1:GLOB:MOD:LOAD "c:\temp\mymodfile.mdx" |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Set and return the state of the specified internal source modulation port. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<bool> |
Choose from: OFF (0) Turn modulation state for specified port OFF. ON (1) Turn modulation state for specified port ON. |
Examples |
SYST:PREF:SOUR1:GLOB:MOD
1 |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal:MODulation[:STATe]? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return the output state of the specified global source. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<bool> |
Choose from: OFF (0) Turn global source output OFF. ON (1) Turn global source output ON. |
Examples |
SYST:PREF:SOUR2:GLOB:OUTP
1 |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal:OUTPut[:STATe]? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return the global sources that ignore the power off setting. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<bool> |
Choose from: OFF (0) Do not ignore power off settings for specified global sources. ON (1) Ignore power off settings for specified global sources. |
Examples |
SYST:PREF:SOUR2:GLOB:POFF:IGN
1 |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal:POFF:IGNore[:STATe]? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-Write) Set and return the power of the specified global source. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<num> |
Global source frequency. Choose any number between the minimum and maximum frequency limits of the analyzer. Units are Hz. |
Examples |
SYST:PREF:SOUR3:GLOB:POW -5 system:preferences:source2:global:power -5 |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal:POWer? |
Return Type |
Numeric |
Not Applicable |
|
Applicable Models: All (Read-Write) Set and return the global state of the specified global source. Learn more. |
|
Parameters |
|
<port> |
Source port number of the VNA. |
<bool> |
Choose from: OFF (0) Turn global state of the specified source OFF. ON (1) Turn global state of the specified source ON. |
Examples |
SYST:PREF:SOUR2:GLOB
1 |
Query Syntax |
SYSTem:PREFerences:SOURce<port>:GLOBal[:STATe]? |
Return Type |
Boolean |
OFF |
|