Preferences


Preferences are settings that survive a Preset or Shutdown.  Preferences are listed on this page with links to locations that provide more information.

How to set Preferences

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press System > System Setup > Preferences....

  1. Click Utility.

  2. Select System.

  3. Select System Setup.

  4. Select Preferences.

 

Preferences  dialog box help  

 

Preferences survive a Preset and a Shutdown.

A checked box makes the following statements true unless stated otherwise.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Avg: On PRESET set two-point group delay aperture (default) - Group delay aperture is set to 11 points.

Avg: On PRESET set two-point group delay aperture - Group delay aperture set to 2 points. Learn more.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Avg: Calculate Group Delay using legacy PNA Math (default) - Do not use legacy group delay aperture computation methods.

Avg: Calculate Group Delay using legacy PNA Math - Use legacy group delay aperture computation methods.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: Always merge when saving Cal in Cal Set (default) - Merge if final cal set covers ≤ 4 ports. In this case, cal sets will be appended. If > 4 ports, erase the existing cal set before saving.

Cal: Always merge when saving Cal in Cal Set - Merge cal sets. This is primarily for multiport systems and can take a significant amount of time to merge.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: Always use Internal Trigger during cal (default) - Only use Internal Trigger source

Cal: Always use Internal Trigger during cal -use the other Trigger source

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: For Frequency Offset, use Primary Frequencies  (default)

Cal: For Frequency Offset, use Primary Frequencies - Use when making mmWave measurements without a test set. Learn more.

This setting only affects calibrations performed using SCPI. Cals performed from the User Interface ALWAYS offer a choice to save to a named Cal Set.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.  

Cal: (SCPI only) Auto-generate a User Cal Set   (default) - Completed calibrations are automatically saved to Cal Registers; NOT to User Cal Sets.

Cal: (SCPI only) Auto-generate a User Cal Set - Completed calibrations are automatically saved to an auto-named User Cal Set. Caution: this can cause a lot of saved User Cal Sets. Learn more.

This is applicable only when the VNA option (160, 161, 260 or 261) is available.

The following message appears when both the Cal Set choices above and below are selected:

"Cal: Auto-save preferences conflict "

Cal: (SCPI) Auto-save to User Cal Set (above)- or - Cal: (SCPI) Auto-save to current Cal Set (below)

Uncheck one of these.

This setting only affects calibrations performed using SCPI. Cals performed from the User Interface ALWAYS offer a choice to save to a named Cal Set.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: (SCPI) Auto-save to current Cal Set - Always automatically save a completed Cal to the Cal Set that is currently selected on the specified channel, which could be the channel Cal Register. If the channel does not yet have a selected Cal Set, the Cal will be saved to a new User Cal Set with an automatically-generated name.

Cal: (SCPI) Auto-save to current Cal Set (default)- Do NOT automatically save a completed Cal to the Cal Set that is currently selected on the specified channel.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: Use legacy behavior for Series-C & Shunt-L fixtures - Legacy operation provided as a user-convenience for backward compatibility. When both of two components of Series-C are set to 0, they are defined as "Short".  when both of two components of Shunt-L are set to 0, they are defined as "Open".

Cal: Use legacy behavior for Series-C & Shunt-L fixtures (default) - Do NOT use legacy operation.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Cal: Use Unknown thru math for SOLT methods - Error terms are computed using the unknown thru method.

Cal: Use Unknown thru math for SOLT methods (default) - Error terms are computed using the definition of the defined thru.

Display: Selected trace changes width briefly. (default) - The selected trace does NOT change width briefly in order to improve visibility.

Display: Selected trace changes width briefly.

Display: Selected Trace is wider.  (default) - The selected trace is the narrow, default size.

Display: Selected Trace is wider. The active (selected) trace is always wider.

Display: Touchscreen ON (default) - Selections can be made by touching the screen.

Display: Touchscreen ON - Selections can NOT be made by touching the screen.

Ext Reference: Modify Settings on PRESET and recall. (default) External reference setting will be maintained by Recall/Preset

Ext Reference: Modify Settings on PRESET and recall. External reference setting will be affected by Recall/Preset

Limit: Draw failed trace segments in red Failed segments are drawn in red. Learn more.

Limit: Draw failed trace segments in red  Failed data points (dots) are drawn in red.

Limit: Draw Limit Lines in Red  Limit lines are drawn in the same color as the trace.

Limit: Draw Limit Lines in Red All Limit limes are drawn in Red.

Limit: Test the nearest measurement point - When the stimulus of measurement point is not the same as the limit test point, the nearest limit test point is used for pass/fail judgement.

Limit: Test the nearest measurement point - The pass/fail is judged at only the stimulus of limit test point.

Markers: Coupling controls on|off state of markers - Turning a marker on or off will have no effect on the markers on other traces.

Markers: Coupling controls on|off state of markers - With Coupled Markers ON, when a marker is turned on, the same-numbered marker on all coupled traces will also be turned on. Likewise, turning off a marker will turn it off on all coupled traces.

Markers: On Preset, Coupled Markers is ON - Coupled Markers is OFF after Preset

Markers: On Preset, Coupled Markers is ON - Coupled Markers is ON after Preset

Markers: On Preset, Coupling Method is Channel - Marker Coupling Method is set to ALL after Preset.

Markers: On Preset, Coupling Method is Channel - Marker Coupling Method is set to Channel after Preset.

Marker: On Preset, set BW/Notch search reference to Peak - BW/Notch marker search reference is set to current marker position after Preset.

Marker: On Preset, set BW/Notch search reference to Peak - BW/Notch marker search reference is set to peak after Preset.

Marker: Programming treats Mkr 10 as Reference  A marker programming command that includes 10 as its marker number argument will operate on the Reference Marker (NOT the general-purpose Marker 10). See Marker commands.

Marker: Programming treats Mkr 10 as Reference  A marker programming command that includes 10 as its marker number argument will operate on the general-purpose Marker 10 (NOT the Reference marker).

Marker: Use single marker for marker search (default) - Use one marker for marker search. Sub Marker is displayed and used for Bandwidth, Notch searches.

Marker: Use single marker for marker search - Use multi marker for marker search.

Memory: Interpolate ON is default condition  Set memory interpolation to OFF as the default.

Memory: Interpolate ON is default condition  Set memory interpolation to ON as the default. Learn more.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Power: On Preset turn power off  Instrument Preset always turns source power OFF.

Power: On Preset turn power off  When the current source power setting is OFF, source power remains OFF after Preset. When the current power setting is ON, source power is turned ON after Preset. Learn more.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Power: On Preset turn power on  Instrument Preset always turns source power ON.

Power: On Preset turn power on  When the current source power setting is OFF, source power remains OFF after Preset. When the current power setting is ON, source power is turned ON after Preset. Learn more.

For SCPI behavior only. Learn more.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Power: Report source unleveled events as errors  Source unleveled events are reported as errors.

Power: Report source unleveled events as errors  Source unleveled events are NOT reported as errors.

Power: Report when receiver is overloaded  A warning message is displayed on the VNA screen indicating that a receiver is overloaded or in compression. The displayed data is probably not accurate. One error per sweep appears and is reported in the Error Log.

Power: Report when receiver is overloaded  Do NOT show overload warnings on the screen or report these errors in the error log.

Preset: Confirm preset - When Preset > Preset is pressed, VNA firmware immediately presets (Hardkey and Softkey are required).

Preset: Confirm preset (default) - When Preset hardkey button is pressed, VNA firmware immediately presets (Hardkey is required only).

Recall: Softkey order is most recently used - Recall softkey order which is most recently used.

Recall: Softkey order is most recently used (default) - Do NOT recall softkey order which is most recently used.

Receiver: On Preset enable auto gain (default) -  Preset makes the receiver gain Auto.

Receiver: On Preset enable auto gain -  Preset does not change the receiver gain setting.

Reference: Modify Settings on Preset and Recall - External Reference settings will be affected by Recall/Preset.

Reference: Modify Settings on Preset and Recall - External Reference settings will be maintained until changed.

Scale: On Preset Couple scale to Window - Scale coupling is set to Window when Preset.

Scale: On Preset Couple scale to Window (default) - Scale coupling is set to Off by default when Preset.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Sweep: On Preset set Sweep Mode to Stepped - Sweep Mode set to Stepped after Preset.

Sweep: On Preset set Sweep Mode to Stepped - Sweep Mode set to Auto after Preset.

This setting is shown only when the VNA option (160, 161, 260 or 261) is available.

Sweep: Use only ramp sweeps for Auto Sweep Mode - Auto Sweep Mode set to use continuous ramp sweeps after Preset.

Sweep: Use only ramp sweeps for Auto Sweep Mode - Auto Sweep Mode set to not use ramp sweeps after Preset.

System: Enable sound (default) - Instrument speaker turns ON.

System: Enable sound - Instrument speaker turns OFF.

System: On Power-on show Keys toolbar - Display softkey toolbar after power-on.

System: On Power-on show Keys toolbar - Hide softkey toolbar after power-on.

System: Use keyboard to navigate softkeys - Enable the keyboard to browse the softkeys.

System: Use keyboard to navigate softkeys (default) - Disable the keyboard to browse the softkeys.

System: Use parallel processing (default) - Enable parallel processing in the CPU which provides higher calculation speeds.

System: Use parallel processing - Disable parallel processing in the CPU.

System: Set front panel remote state when a SCPI command is received - Enable changing from local to remote status when a SCPI command is received.

System: Set front panel remote state when a SCPI command is received -  Disable changing from local to remote status when a SCPI command is received.

DC Source: Use Default for DC Source Initial State - Set the Default setting for the Default DC after preset.

DC Source: Use Default for DC Source Initial State - Default DC setting will be will be maintained until changed.

Phase Noise: Show Power Level of IF signal (default) - Do not display the power level of IF signal.

Phase Noise: Show Power Level of IF signal -  Display the power level of IF signal a the bottom left of screen in parentheses. No change within Residual or External Mixer modes.

 

The More buttons launch dialogs that contain predefined preferences:

Data Saves... -

Define Data Saves - While not explicitly called Preferences, all of these settings survive a shutdown. Learn more.

Power Limit

Offsets and Limits - Sets Power Limits and Offsets. Learn more.

Transparency...

Dialog Transparency - Some dialogs can be viewed in various levels of transparency. Learn more.

Language...

Help - Sets the language of the built-in help (English or other localized language). Learn more.

User Preset...

User Preset - Specify the Instrument State file that the analyzer will use when Preset. Learn more.

Page Setup...

Page Setup - Standard printer settings (Paper, Orientation, and Size) do NOT survive a shutdown.

All other settings DO survive a shutdown. Learn more.

Colors...

Display Colors - Sets display items to custom colors. Learn more.

Print Colors - Sets print items to custom colors. Learn more.

Toolbars...

Show Toolbars/Other Bars - Select toolbars to display.

Defaults - Restore preferences to their default values.

 

Although they are called preferences, the following settings do NOT survive a shutdown.

Calibration

UI Setting

Show or not, the first 'Method' Page of the Cal Wizard.

Cal Preferences

Set and order default Cal Types

Cal Preferences

Perform orientation of the ECal module during calibration?

ECal Wizard

Specify ECal port mapping when orientation is OFF

ECal Wizard

Show or hide custom Cal Windows during Cal

Cal Window (remote commands only)