Security Levels
None - All frequency
information is displayed on the screen and printouts.
Low security level -
Frequency information is blanked from the following:
Display annotation
Calibration properties
All tables
All toolbars
All printouts
External
sources - See Also: Preference
to Deactivate External Devices on Preset. Note: Frequency Blanking
is fully supported ONLY on Keysight MXG sources with option
006. On MXG models without option 006 and all PSG models,
the window state is turned OFF. When the “local” button
is clicked on the source, then frequency is re-displayed.
High security
level - Low security level settings PLUS:
Extra security level
- High security level settings PLUS:
All ASCII data
saving capability (.snp, .prn, .cti) is saved without
frequency information. The X-axis information is replaced
with data point numbers. Before A.08.50, saving these file
types was NOT allowed.
Mixer
setup files (*.mxr) can NOT be saved.
For ALL security levels:
Frequency information is NOT
blanked from the following:
Instrument State and Cal Sets
The security level is always saved and recalled with an instrument
state. However, the instrument state may contain a Cal Set or
link to a Cal Set. Learn
more. This may influence the security level when the instrument
state is recalled. Here is how.
When a new Cal Set is created at the end of
a calibration, the current system security level is stored
with it.
The only way
to change an existing Cal Set’s security level is by writing
a new calibration into the Cal Set.
When later applied to a channel, if the Cal
Set has a higher security
level than the current system security level, the system security
level will become upgraded to that of the Cal Set.
When saving an instrument state to either
a *.csa or *.cst file, the security levels of the system and
Cal Set are saved separately. When recalled, the higher security
level of the two is applied.
To view the security level of a Cal Set, see
Cal Set Properties.
Re-displaying
frequency information
When in Low
security level, do any of the following:
Revisit this dialog box and select
None
Perform an instrument
preset
Recall an Instrument State/Cal
Set with security level of None.
When in High
or Extra security
level, do any of the following:
|
|