Channel Window

Window for displaying the traces. Because a channel corresponds to a window, it is called a channel window. When the outer frame of a channel window is displayed in light gray, it shows that the channel is an active channel (the channel for which setup is being performed). In the following figure, Channel 1 (the upper window) is the active channel. To make a channel active, use Channel Next or Channel Prev. Clicking inside a channel window will also make the channel active.

Channel 1 Window and Channel 2 Window describes different measurement parameters available in the channel measurement window. The measurement parameters described in the Channel 1 and 2 Window correspond to the same channel measurement window and are displayed in separate windows for ease of read.

Channel 1 Window

 

Channel 2 Window

Bandwidth Parameters

Turning on the bandwidth search function displays the bandwidth parameters here.

Channel Number

Indicates the channel number.

Channel Status Bar

The status of each channel is displayed here.

Averaging Status

Displays the averaging factor and averaging count when averaging is turned on.

n/m (displayed in blue)

Averaging: ON
(m: averaging factor; n: averaging count)

(not displayed)

Averaging: OFF

Channel Measurement Status

Displays the update status of traces on the channel.

!

 

Measurement in progress. When the sweep time exceeds 1.5 seconds, ↑  is displayed at the point on the trace.

#

Invalid traces. The measurement conditions have changed, but the traces on the channel currently displayed have not been updated to match the new conditions.

(No display)

The measurement has not been executed.

Error Correction Status

Displays the execution status of error correction on the channel.

 

IF Bandwidth/CW Frequency

Indicates the IF bandwidth when the sweep type is linear/log frequency or the CW frequency when the sweep type is power.

Port Extension Status

Shows whether the port extension and impedance port extension (Option 005 only) or is turned ON or OFF. port extension and impedance port extension can be truned on both at the same time.

PExt (displayed in blue)

Port extension: ON

ZExt (displayed in blue)

Z port extension: ON

(not displayed)

Port extension: OFF

Sweep Range

Indicates the sweep range by using the start/stop or center/span.

Channel Title Bar

You can assign a title to each channel and have the title displayed on the bar.

Data Format

The data format of each trace is displayed here.

See Also: Trace Parameter Display

Graticule Labels

Y-axis divisions in the rectangular display format. When traces in the rectangular display format are overlaid, the Y-axis divisions for the active trace are displayed. The value of the reference line (the division line between and ) is entered numerically by opening the data entry bar using the keys:  Scale > Reference Value. You can change values of the reference line at one-division intervals by placing the mouse pointer in the area of the graticule label (the pointer changes from to ), moving the pointer vertically with the left mouse button pressed, and then releasing the button at the desired location.

Marker Indicators

Indicates the positions of markers on the stimulus axis.
 

Active marker indicator

Non-active marker indicator

You can also move a marker to the desired position by placing the mouse pointer on the marker indicator or position of the marker itself (the pointer changes from to ), moving the indicator vertically with the left mouse button pressed, and then releasing the button at the desired location.

Marker Numbers

Displayed marker number is listed. For the active marker (the one for which setup and analysis are being performed), > is displayed at the left of the marker number. For the reference marker, is displayed instead of the marker number.

Marker Response Values

The marker response value for each marker (the measurement value at the marker point) is displayed here. Two (or three) response values are displayed for data in Smith chart or polar display format.

Markers

The markers used for reading values on a trace. Up to 10 markers can be displayed for each trace.

Active marker (the one for which setup and analysis are being performed)

Non-active marker

Here, "n" denotes a marker number. For the reference marker, however, nothing is displayed at the location of n. Clicking the marker or one of the Marker Indicators makes the marker active.

 

Marker Stimulus Values

The marker stimulus value for each marker (the frequency/power level at the marker point) is displayed here.

Properties

Displays the status of the obtained calibration coefficients on the channel.

Reference Line Indicators

The indicators that indicate the position of the reference line for the Y-axis scale in the rectangular display format. One indicator is to the right and the other is to the left of the scale ( and ). To enter a numeric value for the position of the reference line, open the data entry bar using the keys: Scale > Reference Position. You can also move the position of the reference line by placing the mouse pointer on either of the two reference line indicators (the pointer changes from to .), moving the indicator vertically with the left mouse button kept pressed, and then releasing the button at the desired location (i.e., a drag-and-drop operation).

Scale Settings

The scale setting for each trace is displayed here. This example shows that "10.00dB/" corresponds to 10 dB per division. "Ref 0.000dB" shows that the value of the reference line is 0 dB.

See Also: Trace Parameter Display

Statistics Data

Turning on the statistics data function displays statistics data here.

Trace Name/Measurement Parameter

The names of the traces, such as Tr1, on the channel and their measurement parameters are displayed here. to the right of the trace name indicates the active trace (the trace for which setup is being performed). To make a trace active, use Trace Next or Trace Prev. Clicking the line where the trace name is placed (the mouse pointer changes from to ) also makes a trace active.

See Also: Trace Parameter Display

Trace Number

In the rectangular display format, the trace number is displayed in the same color as the trace at the right end of each trace.

Trace Status Area

The setup for each trace is displayed here.

See Also: Trace Parameter Display

Trace status display

Classification

Contents inside [ ]

Meaning

Error correction

RO

Error correction: ON (OPEN (n) response calibration)

RS

Error correction: ON (SHORT (n) response calibration)

RT

Error correction: ON (THRU (n) response calibration)

ER

Error correction: ON (Enhanced response calibration)

F1

Error correction: ON (1-port calibration )

F2

Error correction: ON (Full 2-port calibration)

Zcor

Error correction: ON Impedance Calibration

Fixture Compensation (Opt 005)

Zcomp

Fixture Compenation ON

Turning on/off traces

Nothing

Data trace: ON, Memory trace: OFF

 

M

Data trace: OFF, Memory trace: ON

 

D&M

Data trace: ON, Memory trace: ON

 

off

Data trace: OFF, Memory trace: OFF

Performing data math

D+M (D+M&M)

Execution of Data+Mem math

When a memory trace is ON, see the contents inside ()

D- M (D- M&M)

Execution of Data- Mem math

 

D*M (D*M&M)

Execution of Data*Mem math

 

D/M (D/M&M)

Execution of Data/Mem math

Electrical delay

Del

A numeric value other than 0 (zero) is specified as the electrical delay or phase offset.

Smoothing

Smo

Smoothing: ON

Gating

Gat

Gating: ON

Fault location

FL(RT)

Fault location: ON, Reflection type: Round Trip

 

FL(OW)

Fault location: ON, Reflection type: One Way

SRL

SRL(xxxΩ)

SRL: ON (xxx is average cable impedance value)

Parameter conversion

Zr

Conversion: ON (Impedance: Reflection measurement)

 

Zt

Conversion: ON (Impedance: Transmission measurement)

 

Ztsh

Conversion: ON (Impedance: Transmission-Shunt measurement)

 

Yr

Conversion: ON (Admittance: Reflection measurement)

 

Yt

Conversion: ON (Admittance: Transmission measurement)

 

Ytsh

Conversion: ON (Admittance: Transmission-Shunt measurement)

 

1/S

Conversion: ON (Inverse S-parameter)

 

Conj

Conversion: ON (Conjugation)

Reference Tracking

PTrk

Peak Track

 

FTrk

Frequency Track

Equation Editor

Equ

Equation Editor: ON

 

Trace Parameter Display

As mentioned above, measurement parameters are displayed at the upper-left of the trace window. However, there is difference in parameter display for network measurement and impedance measurement.

Network Measurement

When network measurement is selected, for example, S11, the following parameters are displayed at the upper-left of the trace window:

Trace number

Measurement Parameter

Format

Scale/Div

Reference value

Impedance Measurement (Option 005)

When impedance measurement is selected, the measurement parameter and format is replaced with Z-parameter and measurement method. Hence, the following parameters are displayed:

Trace number

Impedance (Z)-Parameter

Method

Scale/Div

Reference value

Y-Axis (Log)

Regardless of the measurement parameter, when Log scale is selected at Y-Axis, the following parameters change.

If Linear scale is selected:

Scale/Div

Reference value

If Log scale is selected:

Top xx.xxx

Bottom xx.xxx

Example

Below are examples of several scenarios.

Network Measurement (with Linear Y-Axis):

Network Measurement (with Log Y-Axis):

Z Measurement (with Linear Y-Axis):

Z Measurement (with Log Y-Axis):