Other topics about Setting Control Functions
The serial number and software options of the E5061B can be checked using the following procedure. See Options for the option displayed in this dialog.
Press System > Firmware Revision.
The Firmware Revision dialog is displayed. It provides information about the installed Options, Serial Number, IP Address, Mac Address and USB ID.
The revision number of the firmware installed in the E5061B can be checked using the following procedure.
Press System > Firmware Revision.
The Firmware Revision dialog is displayed.
Press System > Firmware Revision.
The Firmware Revision dialog is displayed.
HDD revision is shown at HDD image.
For more information, refer to HDD Revision History.
At the firmware revision A.1.xx, the HDD revision is not displayed at the Firmware Revision dialog box.
The HDD revision for the revision A.1.xx can be checked using Start > My Computer > C: drive label. For example, the HDD version of the E5061B in the figure below is EL003.