Other topics about Storing Data and Setting
The SnP file format is changed depending on the selected DUT topology.
File Extension |
DUT Topology |
.s1p |
Single Ended 1 |
.s2p |
Single Ended 2, Differential 1 |
.s4p |
Single Ended 4, Differential 2 |
See the Saving data in Touchstone format for touch stone format.
The trace data can be saved in touch stone format.
Click File in the tool bar.
Select Save Touchstone from menu, then the Save Touchstone As Dialog Box is displayed.
Type desired file name.
Click Save.
You can not create touchstone files in the following conditions.
# is displayed at Channel Measurement Status.
Some cases in Advanced Mode with Advanced Calibration Method