Channel Window

Windows for displaying traces. Because a channel corresponds to a window, it is called a channel window. When the outer frame of a channel window is displayed in light gray, the channel is the active channel (the channel for which setup is being performed). In the following figure, Channel 1 (the upper window) is the active channel. To make a channel active, use Channel Next or Channel Previous key. Clicking inside a channel window will also make the channel active.

Channel 1 Window

Channel 2 Window

Channel Title Bar

You can assign a title to each channel and have the title displayed on the bar. For more on setting up a channel title bar, see Labeling a window.

Trace Name/Measurement Parameter

The names of the traces (Tr1 through Tr9)on the channel and their measurement parameters are displayed here. to the right of the trace name indicates the active trace (the trace for which setup is being performed). To make a trace active, use Trace Next Key or Trace Prev Key. Clicking the line where the trace name is placed (the mouse pointer changes from to ) also makes a trace active.

Data Format

The data format of each trace is displayed here. For more on setting up data formats, see Selecting a Data Format.

Scale Settings

The scale setting for each trace is displayed here. This example shows that "10.00dB/" corresponds to 10 dB per division. "Ref 0.000dB" shows that the value of the reference line is 0 dB. For more on setting scales, see Setting the Scales.

 

Shift LO Status

Displays the Shift LO status on the channel.

Trace Status Area

The setup for each trace is displayed here.

Trace status display

Classification

Contents inside [ ]

Meaning

Error correction

(In the option TDR, this information should be ignored.)

RO

Error correction: ON (OPEN (n) response calibration)

RS

Error correction: ON (SHORT (n) response calibration)

RT

Error correction: ON (THRU (n) response calibration)

ER

Error correction: ON (Enhanced response calibration)

F1

Error correction: ON (1-port calibration )

F2

Error correction: ON (Full 2-port calibration / 2-port TRL calibration)

F3

Error correction: ON (Full 3-port calibration / 3-port TRL calibration)

F4

Error correction: ON (Full 4-port calibration / 4-port TRL calibration)

Turning on/off traces

Nothing

Data trace: ON, Memory trace: OFF

M

Data trace: OFF, Memory trace: ON

D&M

Data trace: ON, Memory trace: ON

off

Data trace: OFF, Memory trace: OFF

Performing data math

D+M (D+M&M)

Execution of Data+Mem math

When a memory trace is ON, see the contents inside ()

D- M (D- M&M)

Execution of Data- Mem math

 

D*M (D*M&M)

Execution of Data*Mem math

 

D/M (D/M&M)

Execution of Data/Mem math

Electrical delay

Del

A numeric value other than 0 (zero) is specified as the electrical delay or phase offset.

Smoothing

Smo

Smoothing: ON

Gating

Gat

Gating: ON

Parameter conversion

Zr

Conversion: ON (Impedance: Reflection measurement)

 

Zt

 

Conversion: ON (Impedance: Transmission measurement)

 

Ztsh

Conversion: ON (Impedance: Transmission-Shunt measurement)

 

Yr

Conversion: ON (Admittance: Reflection measurement)

 

Yt

Conversion: ON (Admittance: Transmission measurement)

 

Ytsh

 

Conversion: ON (Admittance: Transmission-Shunt measurement)

 

1/S

Conversion: ON (Inverse S-parameter)

 

Conj

Conversion: ON (Conjugation)

Power correction

PC

Error correction: ON (Power calibration)

Receiver correction

RC

Error correction: ON (Receiver calibration)

Scalar-mixer correction

Cor

Error correction: ON (Scalar-mixer calibration)

Equation Editor

Equ

Equation Editor: ON

 

5-6. Reference Line Indicators

The indicators that indicate the position of the reference line for the Y-axis scale in the rectangular display format. One indicator is to the right and the other is to the left of the scale ( and ). To enter a numeric value for the position of the reference line, open the data entry bar using the keys: Scale > Reference Position. You can also move the position of the reference line by placing the mouse pointer on either of the two reference line indicators (the pointer changes from to .), moving the indicator vertically with the left mouse button kept pressed, and then releasing the button at the desired location (i.e., a drag-and-drop operation).

5-7. Trace Number

In the rectangular display format, the trace number is displayed in the same color as the trace at the right end of each trace.

5-8. Properties

 

Displays the following properties.

Property Name

Description

Calibration Property

Displays the status of the obtained calibration coefficients on the channel. For details, see Acquisition status of calibration coefficient for each channel.

E5091A Property

Displays the assignment information of the test ports on the channel. For details, see Displaying the multiport test set properties.

Balanced Measurement Topology Property

Displays the topology for balanced measurement on the channel. For details, see Checking device type and port assignment.

5-9. Channel Status Bar

The status of each channel is displayed here (see parts 5-10 through 5-16).

5-10. Channel Measurement Status

Displays the update status of traces on the channel.

!

 

Measurement in progress. When the sweep time exceeds 1.5 seconds, ↑  is displayed at the point on the trace.

#

Invalid traces. The measurement conditions have changed, but the traces on the channel currently displayed have not been updated to match the new conditions.

(No display)

The measurement has not been executed.

5-11. Error Correction Status

Displays the execution status of error correction on the channel. For details, see Execution status of error correction for each channel.

5-12. Power Calibration Status

Displays the execution status of power level error correction on the channel. For details, see Turning Power Level Error Correction ON/OFF.

5-13. Port Extension Status

Shows whether the port extension is turned ON or OFF.

PExt (displayed in blue)

Port extension: ON

(not displayed)

Port extension: OFF

5-14. Fixture Simulator Status

Shows whether the fixture simulator is turned ON or OFF.

Sim (displayed in blue)

Fixture simulator: ON

(not displayed)

Fixture simulator: OFF

5-15. Averaging Status

Displays the averaging factor and averaging count when averaging is turned on.

n/m (displayed in blue)

Averaging: ON
(m: averaging factor; n: averaging count)

(not displayed)

Averaging: OFF

5-16. Sweep Range

Indicates the sweep range by using the start/stop or center/span.

5-17. IF Bandwidth/CW Frequency

Indicates the IF bandwidth when the sweep type is linear/log frequency or the CW frequency when the sweep type is power.

 

5-18. Channel Number

Indicates the channel number.

5-19. Graticule Labels

Y-axis divisions in the rectangular display format. When traces in the rectangular display format are overlaid, the Y-axis divisions for the active trace are displayed. The value of the reference line (the division line between and ) is entered numerically by opening the data entry bar using the keys:  Scale Key + Reference Value. You can change values of the reference line at one-division intervals by placing the mouse pointer in the area of the graticule label (the pointer changes from to ), moving the pointer vertically with the left mouse button pressed, and then releasing the button at the desired location.

5-20. Bandwidth Parameters

Turning on the bandwidth search function displays the bandwidth parameters here. For more on the bandwidth search function, see Determining the Bandwidth of the Trace (Bandwidth Search).

5-21. Marker Numbers

The marker values are displayed in a list at positions 5-21, 5-22, and 5-23. Position 5-21 displays the marker numbers. For the active marker (the one for which setup and analysis are being performed), > is displayed to the left of the marker number. For the reference marker, is displayed instead of the marker number.

5-22. Marker Stimulus Values

The marker stimulus value for each marker (the frequency/power level at the marker point) is displayed here.

5-23. Marker Response Values

The marker response value for each marker (the measurement value at the marker point) is displayed here. Two (or three) response values are displayed for data in Smith chart or polar display format.

5-24. Markers

The markers used for reading values on a trace. Up to 10 markers can be displayed for each trace.

Active marker (the one for which setup and analysis are being performed)

Non-active marker

Here, "n" denotes a marker number. For the reference marker, however, nothing is displayed at the location of n. Clicking the marker or one of the Marker Indicators makes the marker active.

 

5-25. Marker Indicators

Indicates the positions of markers on the stimulus axis.
 

Active marker indicator

Non-active marker indicator

You can also move a marker to the desired position by placing the mouse pointer on the marker indicator or position of the marker itself (the pointer changes from to ), moving the indicator vertically with the left mouse button pressed, and then releasing the button at the desired location.

5-26. Statistics Data

Turning on the statistics data function displays statistics data here. For more on the statistics data function, see Determining the Mean, Standard Deviation, and p-p of the Trace