SCPI.CALCulate(Ch).XXXX.PARameter.TNAMe.XXXX

As mentioned in Selecting the Active Channel/Trace, if you are using E5071C revision A.9.60 and above, you can select a trace by the trace name, provided it has been defined earlier. To define a trace name, use the following command:

:CALC{[1]-160}:PAR{[1]-16}:TNAMe:DATA

If the trace name is not defined but used, the following error occurs:

'51, Specified trace does not exist'

If the defined trace name already exist, the following error occurs:

'63, Duplicate trace name'

 

The following commands allow you to select the active trace directly by using TNAMe:

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAME.BALanced.DEFine

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAME.BBALanced.DEFine

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAME.SBALanced.DEFine

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAME.SSBALanced.DEFine

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAME.STATe

SCPI.CALCulate(Ch).PARameter.TNAME.DEFine

SCPI.CALCulate(Ch).PARameter.TNAME.SELect

SCPI.CALCulate(Ch).PARameter.TNAME.SPORt